Other Parts Discussed in Thread: UCC27528
Hi TI Team I need your help!
I am currently using the UCC27528 within an IGBT gate drive application however I have identified some issues regarding the device enable pin voltage threshold.
The design arrangment is such that both input pins INA and INB are pulled up to VDD and the enable pins ENA and ENB are tied together and connected to an input PWM waveform (Low Level TTL 3.3V). As expected the device outputs the PWM trace given a 3.3V input waveform however when the input waveform voltage is taken to 3.1V the output drops off to 0V. The datasheet states that VEN_H should be 2.1V however it seems to be much higher. Is anybody able to shed any light on why the device exhibits the described operational characteristics?
Thanks in advance …
Luke Ashton