This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Paralleling Power Mosfets in linear mode

Other Parts Discussed in Thread: TL081

We are using 3 Power Mosfets IXTX40P50P  in parallel and driving them through an Op amp TL081 in a current source of 0-5 A. The sources are tied and are supplied with 25 V through a sense resistor of 1 Ohm. The gate resistors placed between op amps output and gates of individual mosfets are 1 K each. The problem is we are getting oscillations at common drain terminal. The load is 5 Ohms. The reference voltage to set current is giving to op amp as a pulse through an anolog switch. How can we eliminate peak overshoots  in output current pulse at drains.

Thank you.