Hello,
I want to use the LM26003 for a design with a GSM / GPRS modem. The application is suitable? peak current required to 30mA to 3A PWM / fPWM function will be a problem? I do not know if fPWM switching PWM mode to be fast enough for a transmission peak.
the "sleep mode", the "PWM / fPWM" function and the "CCM / DCM" function is the same? What is the difference?
The manufacturer of GSM / GPRS modem advises: "Power supply quality
PFM, or PSM systems Should be avoided; Low ripple, linear regulation or PWM converters are preferred for low noise. "
I'm also considering LMZ13608, LMZ14203 and LMR14050 but I'm not sure that's the right application.
Efficiency is important but necessary to 50mA peaks up to 3A and low ripple and noise.
Thanks you