Hello all
I'm trying the drive IPP60R099C7 power mosftet in PFC boost stage with Switching frequency equal to 125kHz. . This Mosfet Qg is 45nC and I believe either UCC27511, UCC27519 can easily drive it. Both UCC27511, UCC27519 cost the same and come with SOT-23 package and have similar output current capabilities (4 amps for both) . . The UCC27519 has enable feature but UCC27511 can also be configured to have enable capability also. The UCC27511 has a great advantage of split output so resistors with different values can be used for turn on and turn off . It will save at least one schottky diode and more space so that driver can be positioned closer to Mosfet to minimize EMI issue. Now the question is that while UCC27511 offering such great advantage why somebody want to use UCC27519? What I'm missing here? Is there a limitation with UCC27511 that I'm not aware of?