I'm using LM43600PWP evaluation board to step down my output voltage. The input voltage is expected to be something between 4-12 DC volts, and the output voltage should be 3.3V. The output of this buck converter is feeding a load of V(load)= 3.3V and I(load)= 13.33x10^6 A. I've seen some equations to adjust the output voltage in LM43600 datasheet; however, I'm I don't know how I can apply those equations to the LM43600 , that is inside the evaluation board LM43600PWP ? Where to start? And are there any any commanded tools or any preferred programmable language? Thanks in advance.
Omar