Other Parts Discussed in Thread: TPS62120, TPS62745
I'm using a TPS62120 converter to regulate a 12V input down to a 3V output. My system draws about 100uA quiescent from its 3V rail, and the datasheet indicates about 70% efficiency there. I thus expect about 100uA * (3 / 12) * (1 / 0.7) = 36uA of current flowing into the buck converter if the TPS device didn't draw any of its own current. I actually measure about 200uA. Is the difference caused by the TPS active-mode current?
The TPS62120 specification calls for a 240uA typical active mode current consumption. Is this something I would see at Iout = 100uA? Is this current factored into the overall efficiency?