When thermal shutdown (or even temporary output short) the output voltage drops to something like 0.5V but the inductor and the associated capacitor get very hot and prevent the regulator from recovery even after a power cycle, or at least until the inductor has cooled significantly. It would appear that the thermal shutdown protects the IC but does something odd to induce the inductor/cap to get very hot. I believe I'm using a bog-standard application circuit but is there something I'm doing wrong to cause this problem?