This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq76200's DSG pin issue

Other Parts Discussed in Thread: BQ76200

Hi , 

I use the bq76200 on 6S battery pack , Attached is my circuit and layout .

Enable DSG_EN pin , I'm going to measure the output voltage on bq76200's DSG pin . The voltage is fail  , tat time is 34V and at time is 6.5V ...  

  • Hi  Pan,

    (1) Please check , if Charge Pump is ENABLED all the time.

    (2) CHG and DSG pin can drive a load C= 10nF. With paralleling of FET, capacitance  will add up. Hence , you may want

    to select  a series resistance to the gates .   Q= I T ; you will need to comprise the rise-time for a clean Turn ON /Off.

    Please send a scope capture and trigger from the  DSG-EN to the DSG  

    hope this helps.