Hi! I'm working with 2 TPS63021 in my design. One, it is for 5V outputs (IC1) and the other is for 3.6V (IC2).
I have problem when the 2 ICs are working. The IC2 works perfect but the IC1 has a short circuit in inductance pins.
When i don't use IC2, IC1 works perfect.
I supose the problem is about the location of my inductors.
Can u help me with my design? Is it correct the location of the both inductors?
-IC1 is on bottom side and IC2 is on top side.
Thank so much,
Javier