I need a dual supply solution with the following specs:
- 8 - 75V input
- 2 outputs:
- non-isolated 12V 20mA
- isolated 12V 50mA
- Automotive rated
- Small as possible
- low-cost (of course)
I am thinking of the LM25118-Q1 with a coupled inductor output, but I'm not sure if that's the best answer...
Any help is appreciated.