Thanks for quick feedback. I need to come up with a solution (may be SW) as there over 2K boards built. A few questions
1) VBATREG spec is not clear in BQ24278. Why 2 values for TA=25?
2) You say Power Cycle the IC. Does this mean to remove and insert power to IN pin while battery is still connected as long as battery voltage threshold is met?
3) Is there any SW solution to this Like toggling CD or CE?
4) Will the 6 hour timer unlatch the CHG pin when you get into this condition?
5) The condition of VBAT > VBATREG-VRCH is ALWAYS the case when you charge a battery to full, NO? Meaning that this device ALWAYS gets into this condition. If yes, wouldn't this device be useless. Why has this not been documented before. Seems to me like a fundamental flaw.
I really need a solution ASAP. Any help is appreciated