Hi,
just to be sure to correctly understand the specifications of TPS62153 ...
The step down converter TPS62153 with output voltage fixed to 5V works also in boost mode if the input voltage is under 5V? For example if the input voltage is between 3V and 5V does it works as a step-up converter in order to have a regulated 5V in output?
Greetings
Attilio