Hi.
I am using the isolated DC/DC converter DCP021212D. And I am not clear about the parameters listed in the datasheet.
1) In section 5 of the datasheet, Device Comparison Table, the barrier capacitance is measured at Viso = 750 Vrms. But according to the section 7.5 Electrical Characteristics, the chip can only sustain continuous 42.5 VAC or 60 VDC. If the Viso is 750 Vrms, the chip can not survive. Does it mean the capacitance was measured within 1 seconds?
2) In the section 7.5. The difference between 1-second flash test voltage and continuous working AC voltage. If I apply on the chip a continuous voltage, but it is several kHz square waveform, which parameter should I use?
Thanks
Boxue