Dear Designers and TI support,
I need to zero the ILED when VIADJ is 0. To do that ROFF has to be connected between Vout and CS. There are 2 equations to to calculate ROFF
Setting Vout = 24V (3Vx8LED = 24V), RF=475 Ohm (demo board) RCS=0.2Ohm (demo board) delta ILED=3mA (for example), It results:
ROFF = min [15.5K, 1.1MEG] so ROFF has to be set to 15.5K.
If I do that 15.5K the VOUT ILED is always 0 even varying VIADJ from 0 to 1V. If I set ROFF to 1.2MEG the linearity is good and only if I set 0V as VIADJ ILED is 0. Starting from VIADJ = 0.1V than the ILED is linear with VIADJ. So the conclusion is the above ROFF selection seems to be wrong and only the max (not min) rule has to apply.
-
Are you sure of the above formula ?
-
Connecting ROFF to VCS produces a down shift of the line ILED = k*VIADJ + q, changing the q value. Unfortunately VOUT is not exactly constant so theoretically “q” is not constant. Why don’t connect ROFF to a constant voltage to increase the regulation linearity ?
Thanks
Paolo