I am usning LP38855 LDO for 1.2V. I am giving a supply of 3.3V at input pin of LP38855.
My question is for bias pin of LP38855; this pin should be connected to Vin (3.3V) directly or i need to connect it through some resistor?
I have gone through the reference design and it is suggested to use 10uF ceramic capacitor between Bias pin and ground. it is also mentione that current drawn from bias pin is very low. so should i need to pull bias pin up to 3.3V?
Thanks