A review of a Worst Case Analysis revealed that an LM117HVHRLQMLV can have a transitory overvoltage condition applied where in Vin - Vout > 60 V. For a set 15V output, nominal Vin is 38 V, Iout is 22 mA. For a period of 10 microseconds, Vin might surge to 75.2 volts.
The concern is that this may damage the device. Understand that operating parameters are not guaranteed for out of spec operating conditions; but will this cause some latch-up or other induced failure? This sort of thing cannot be modeled reliably as the existing models work on optimal parameters - even the schematic supplied does not reflect the true design. This is, I think, process related.
Thoughts?