Hi,
What are the internal resistor values tied to the INH pin in a TPS84610 device? I am currently using an open drain buffer, 74LVC2G07, connected to the IHN pin and I want to make sure this open drain device is not causing unintended glitching on the output. From the datasheet, INH pin "has an internal pullup. Do not place an external pull-up resistor on this pin. If this pin is left open circuit, the device operates when input power is applied. A small low-leakage MOSFET is recommended for control. See the application section for further guidance."
What is the maximum leakage value for the MOSFET? Does my open drain buffer meet the spec?
In advance, thank you.