This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Parallel Current Sharing using DCR021205's

Other Parts Discussed in Thread: DCR021205

Sorry this is in the wrong forum but I could not find a Isolated DC/DC section.

 

I require an isolated power system to power a microcontroller, 4 Optocouplers, and some various sensors, approximately 3W.

 

One DCR02 is capable of 2W output Max.

 

My problem is that there isnt a isolated dc/dc converter that can meet these power requirements, so i'm electing to put two DCR021205 in parallel to share the load in order to give me the output power that my design requires.

 

I'm wondering if there are any design consideration i should take into consideration other than whats outlined in the application sheets as too noise reduction and low external capacitance on the sync pins of the device.

 

This is being implemented on a 4 Oz/Cu PCB with 90mil traces.

 

Cheers,

Justin