Hi,
I'm looking to using tps54418 for a low drop operation which consist of 5.5Vin, 5.2Vout, 3.5A=Iout, Fsw=1MHz.
I have used and tuned the standard tps54418EVM to do some preliminary measurements in order to validate the concept.
I have started the tps54418 at light load and the setup seems to work fine HOWEVER when I increase the load, Fsw fold back to around 333kHz for Iout=3.5A (full load condition).
- This frequency-foldback is mentioned for the startup and OC (over current) in the datasheet, but nothing say that it could happen as well when we hit close to 100% duty cycle. So it’s a bit ambiguous…
- I saw another information in the datasheet which indicates that the tps54418 can work up to 100% dutycyle as long as the Boot to PH voltage doesn't drop below the Boot UVLO threshold. For tps54418: Vuvlo(boot)=2.1V typ for Vin=3.95V. So I have measured the Boot to PH voltage, see below.
Blue trace = BOOT to GND
Yellow trace = PH to GND
Note = We clearly see that the 2 switching cycles on the left are at 500kHz (Fsw/2), then the 3rd one is around 333kHz (Fsw/3).
Looking at the screenshot above it doesn’t seem that the Bootstrap capacitors isn’t charged enough. So no problem to be foreseen from this side...
Therefore I would suppose that the internal frequency foldback is causing this frequency shift.
Could you comment and put some lights on this mode of operation? it's not clear when this frequency fold back can happen and which Fsw is then applied on the Switching Node.
Thanks and best regards,
-nico