Hi all!
I'm using TPS60110 in my board to step up voltage from lithium battery to 5V. Iout is around 90mA and supply two isolated DCDC ROE0505 and one SP485 all bypass with 22uF MLCC 0805 cap.
After start time all works well. I can't understand what happens during start.
I execute some test only with TPS60110 and 22uF MLCC on output, NO LOAD. Below picture from oscilloscope.
In blue the ouput voltage of TPS60110 and in red the voltage after 300mOhm resistor between voltage source of(4.39V) and TPS input.
Trigger on enable rise edge. Time division 200uS/div.
So during voltage rise current follow it with ohmic law, until about 190mA, after happen an abrut current increase until 1.6A without LOAD. Can you explain why it happen? Who will use all that power? Datasheet says that IoutMax should be 300 mA, without current protection circuit only with short protection.
I try the same circuit with TPS60150 that expose soft start circuit with 150uS time rise. This is the result with FULL LOAD:
I expect an time rise of 150us but i measure 0.7us. Can you explain what happens? I think at start short protection circuit limit output current at 60/70 mA but that protection should disable after output rise of some volt, so why it don't delivery all current of 140mA what limit output current?
Thanks
Marco