Hi, I built an LED driver using the WEBENCH tools and the design is attached here. When I try and simulate this design in TINA-TI, I dont get the outputs I'm looking for. What am I missing here? Both are attached here.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, I built an LED driver using the WEBENCH tools and the design is attached here. When I try and simulate this design in TINA-TI, I dont get the outputs I'm looking for. What am I missing here? Both are attached here.
OK. How do I then simulate a custom LED? I tried editing the LED configurations in the steady state schematic but it says its encrypted. The Vf of my LED is 2.6V and If is about 250mA. I wanted to connect 6 parallel chains with each chain containing 2 of these in series giving me 5.2V and 1.5A at the output.
I've attached the schematic with the Zener as the load and it does not seem to be working. I still see the full Vin at Vo and the load current is barely about 300mA. Ron, Cin, Cout and duty cycle are all calculated using the formulas given in the datasheet. Any help would really help.
I have no idea when they can get around to looking at it, they are very busy and it may take a long time. But your circuit should work well as long as you follow good layout guidelines.