This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Could you tell me about TPS62240's output voltage accuracy?

Other Parts Discussed in Thread: TPS62240, TPS62560, TPS62097

Hello.
My customer is currently in using TPS62240,now.

<Question>

1. The customer have requested that is fit to ±3.0% at output voltage accuracy(within including the Ripple),while maintaining a high efficiency(must PFM Mode).

   What percentage is the output voltage accuracy at the time of PFM Mode operation in the worst case?

By the way , that VFB accuracy will be fit to ± 3.0% is confirmed


< Customer specification conditions >
VIN: 5.0V ± 3.0%
VOUT: 3.1V ( less than ± 3.0%)
※ RFB1 / RFB2 using ± 0.5% resistance accuracy
IOUT: 0.1A@MAX
COUT = 10uF
Temp: -40 ~ 125 ℃

2. Also, I have that this(TPS62240 / TPS62560) was heard the same Chip.

     Does TPS62240 have a DVP (Dynamic Voltage Positioning)?

Could you help us?

Best Regards,

Pokkun