Dear Sir or Madam.
We are going to use boost controller TPS43061 and MOSFET CSD16340Q3 in battery charger. In this application this controller will work at different input and output conditions and we would like to simulate it. Is it possible to get unencrypted model for these parts? As we are using SIMPLIS simulator for frequency respond analysis, we would like to create our own model of TPS43061 and we need some information which can not be found in Datasheet:
- Gain of Sense Signal Amplifier:
- Slope Compensation Signal parameters.
Also, TPS43061 Datasheet says, that it is optimized for low Qg , but the Datasheet does not have any current limit for gate drive. We tested this IC with MOSFETs which have Qg=63nC (max) and Ciss=10000pF (max). Peak Drive current for this MOSFETs was +-1.5A for Low and +-1A for High MOSFET. We could not see any problem for these conditions (in terms of functionality , components stress and temperature). Do you think it will not create any problem for TPS43061?
Thanks