This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Ramp down limitation on UCD9244

Other Parts Discussed in Thread: TMS320C6657, UCD9244, UCD74106

I'm using a UCD9244 along with 3 UCD74106 devices to supply power to a TMS320c6657 for the CVDD, CVDD1, and DVDD15 supply voltages and for whatever reason I can’t get them to ramp down faster than ~2ms, I can make it longer than 2ms but not shorter, we will need a much faster ramp down than that for our hot plug application.  I have determined that the problem is not a dv/dt discharge current issue, an under current issue, or a 3.3V power supply issue.  It’s like there is a global ramp down limit that I’m running into and I searched the data sheet and user guide with no success.  Do you have any suggestions?