Other Parts Discussed in Thread: BQ24270
I'm trying to understand better the behaviors of the bq24270 in its various low-power modes. The triggers for those modes appear to be the CD input, the level of incoming power (VUSB), and the /CE bit in the Control Register.
1. Are the CD input and the /CE bit identical, or is there a difference?
2. Do CD and /CE have any effect if VUSB is below the undervoltage threshold?
3. Is there any problem with logic high levels being present on SCL, SDA, etc. when VUSB is not present?
Thanks,
Scott