I am using the PTB48580B and PTB48580A Isolated DC/DC converters with a common 54VDC input. All of the outputs (+/-12, +/-5) have at least 200mV ripple at about 1.25MHz. I can see a spike at about 480kHz which must correspond to the switching frequency, but I do not know where this 1.25MHz ripple is coming from. At each output, I have a 10uF tantalum cap in parallel with a 1uF tantalum and a 0.1uF ceramic chip capacitor. I see from the datasheet that a very low ESR capacitor can cause instability, but I do not believe that any of these capacitors have low ESR. Are there any other design or layout considerations I would need to follow in order to avoid this large ripple?
From the datasheet, switching frequency synchronization is necessary when using the PTB48580 with a PTB4850x to prevent adding a beat frequency to the ripple components from the converters. Could it be that using two PTB48580's without synchronizing them is causing this problem? Or is synchronization only an issue when used with the PTB4850x?
Any suggestions would be greatly appreciated. Thank you in advance for your help!