Is it possible to adapt UCC287004 to work from 3-PH 440V RMS system. Specifically, will UCC28704EVM-724 10-W USB Adapter evaluation board work in this application assuming the AC LINE input components are rated for 1200V. Also, a six diode bridge with 100nF bulk capacitor is used. Would the transformer used in the evaluation board work at 600V, if not do you have a recommendation. Would you recommend a different controller? It has to simple as UCC28704.
Thank you for your help
Silvo