The spec for the TPS53915 describes I-VDD as 1850uA-max, but with "Power conversion enabled (no switching)". Not sure what this means and I need to know what the maximum VDD current is when there is switching. 1850uA seems too low - I was expecting more to drive the internal top and bottom FET gate capacitance. And it should be frequency dependent as well. My switching frequency is 1MHz.