This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63061 Vout

Genius 4840 points
Other Parts Discussed in Thread: TPS63061, TPS63060

Please let us know TPS63061 Vout accuracy when VPS/SYNC=Vin.

I only found  Vout accuracy when  VPS/SYNC=GND in datasheet Page5.

www.tij.co.jp/.../tps63061.pdf

Regards,

  • Looking at Page 10 of the datasheet, it seems the output voltage during PFM has a fixed hysteretic swing(turned on/off) based on a comparator's threshold as the converter actually stops operating at low loads. During regular operation at loads >100mA, the device is in PWM mode and the Vout accuracy depends on the device's voltage ripple which is dependent on the frequency of the device, output capacitance, etc.
  • This should be the same 1% accuracy as the adjustable TPS63060 IC.