Hello, I am using the Bq25101H to charge at a max rate of 36mA. Everything works as it should except the !CHRG pin doesn't go low when the battery current drops below 10% in the voltage regulation and charge termination phase. We observed the charging current go from 36mA down to 1mA, and the !CHRG remains low.
Notes:
1) We are using an internal pullup on a processor pin to pull !CHRG high during high impedance state.
2) The datasheet mentions that for charge rates below 50mA, an RC filter should be used across the ISET resistor. We tried with this filter and the issue is still there.
Thanks,