HI.
Now, I'm trying to test with PTH05050WAH module.
PTH05050WAH |
MODULE PIP .8-3.6V 6A HORZ T/H |
My power source is SMPS 5V 2A adaptor and I connect directly the 5V power source of adaptor to 3 pin of PTH05050WAH module and 1pin to GND.
Here is Problem, When I check the output voltage of PTH05050WAH module by multi voltage meter.
I've got 0.7V with 2.48K ohm( It's original module's resistor).
As I know, when we use 2.48K ohm, then the output voltage supposed to be 2.40~2.45V.
But in my case I've got only 0.7. I can't understand.
Does anyone know what is gong on? and let me know why does it difference between PDF's and real measure voltage