This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5007/LM5008/LM5009 won't regulate and runs hot



Hi,

I am using the LM500x series to buck a 48V battery down to 5V, however whenever the converter is loaded it will not regulate its output voltage correctly and it will sink a significant current resulting in the converter running very hot. Whenever I power the circuit externally there is no problem. Schematic is shown below. The converter does regulate correctly when no load is connected. The load current averages about 65mA.