Other Parts Discussed in Thread: LM3642, LM3644
Hi,
My customer use LM3644TT, but they do not know how to initial the communication with Qualconn chip.
Do We have reference initial code for Qualconn platform?
Now they are testing LM3642 initial code. Is it OK?
(They will revise register code because LM3644TT and LM3642 has different register map. They just need initial code, and build up the bridge to main chip)
Thanks
/* Copyright (c) 2014-2015, The Linux Foundation. All rights reserved.
*
* This program is free software; you can redistribute it and/or modify
* it under the terms of the GNU General Public License version 2 and
* only version 2 as published by the Free Software Foundation.
*
* This program is distributed in the hope that it will be useful,
* but WITHOUT ANY WARRANTY; without even the implied warranty of
* MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
* GNU General Public License for more details.
*
*/
#include <linux/module.h>
#include <linux/export.h>
#include "msm_camera_io_util.h"
#include "msm_led_flash.h"
#define FLASH_NAME "ti,lm3642"
#define CONFIG_MSMB_CAMERA_DEBUG
#ifdef CONFIG_MSMB_CAMERA_DEBUG
#define LM3642_DBG(fmt, args...) pr_err(fmt, ##args)
#else
#define LM3642_DBG(fmt, args...)
#endif
static struct msm_led_flash_ctrl_t fctrl;
static struct i2c_driver lm3642_i2c_driver;
static struct msm_camera_i2c_reg_array lm3642_init_array[] = {
{0x0A, 0x00},
{0x08, 0x07},
{0x09, 0x19},
};
static struct msm_camera_i2c_reg_array lm3642_off_array[] = {
{0x0A, 0x00},
};
static struct msm_camera_i2c_reg_array lm3642_release_array[] = {
{0x0A, 0x00},
};
static struct msm_camera_i2c_reg_array lm3642_low_array[] = {
{0x0A, 0x22},
};
static struct msm_camera_i2c_reg_array lm3642_high_array[] = {
{0x0A, 0x23},
};
static const struct of_device_id lm3642_i2c_trigger_dt_match[] = {
{.compatible = "ti,lm3642"},
{}
};
MODULE_DEVICE_TABLE(of, lm3642_i2c_trigger_dt_match);
static const struct i2c_device_id lm3642_i2c_id[] = {
{FLASH_NAME, (kernel_ulong_t)&fctrl},
{ }
};
static void msm_led_torch_brightness_set(struct led_classdev *led_cdev,
enum led_brightness value)
{
if (value > LED_OFF) {
if(fctrl.func_tbl->flash_led_low)
fctrl.func_tbl->flash_led_low(&fctrl);
} else {
if(fctrl.func_tbl->flash_led_off)
fctrl.func_tbl->flash_led_off(&fctrl);
}
};
static struct led_classdev msm_torch_led = {
.name = "torch-light",
.brightness_set = msm_led_torch_brightness_set,
.brightness = LED_OFF,
};
static int32_t msm_lm3642_torch_create_classdev(struct device *dev ,
void *data)
{
int rc;
msm_led_torch_brightness_set(&msm_torch_led, LED_OFF);
rc = led_classdev_register(dev, &msm_torch_led);
if (rc) {
pr_err("Failed to register led dev. rc = %d\n", rc);
return rc;
}
return 0;
};
int msm_flash_lm3642_led_init(struct msm_led_flash_ctrl_t *fctrl)
{
int rc = 0;
struct msm_camera_sensor_board_info *flashdata = NULL;
struct msm_camera_power_ctrl_t *power_info = NULL;
LM3642_DBG("%s:%d called\n", __func__, __LINE__);
flashdata = fctrl->flashdata;
power_info = &flashdata->power_info;
gpio_set_value_cansleep(
power_info->gpio_conf->gpio_num_info->
gpio_num[SENSOR_GPIO_FL_NOW],
GPIO_OUT_LOW);
if (fctrl->flash_i2c_client && fctrl->reg_setting) {
rc = fctrl->flash_i2c_client->i2c_func_tbl->i2c_write_table(
fctrl->flash_i2c_client,
fctrl->reg_setting->init_setting);
if (rc < 0)
pr_err("%s:%d failed\n", __func__, __LINE__);
}
return 0;
}
int msm_flash_lm3642_led_release(struct msm_led_flash_ctrl_t *fctrl)
{
int rc = 0;
struct msm_camera_sensor_board_info *flashdata = NULL;
struct msm_camera_power_ctrl_t *power_info = NULL;
LM3642_DBG("%s:%d called\n", __func__, __LINE__);
if (!fctrl || !fctrl->flashdata) {
pr_err("%s:%d fctrl NULL\n", __func__, __LINE__);
return -EINVAL;
}
flashdata = fctrl->flashdata;
power_info = &flashdata->power_info;
gpio_set_value_cansleep(
power_info->gpio_conf->gpio_num_info->
gpio_num[SENSOR_GPIO_FL_NOW],
GPIO_OUT_LOW);
if (fctrl->flash_i2c_client && fctrl->reg_setting) {
rc = fctrl->flash_i2c_client->i2c_func_tbl->i2c_write_table(
fctrl->flash_i2c_client,
fctrl->reg_setting->release_setting);
if (rc < 0)
pr_err("%s:%d failed\n", __func__, __LINE__);
}
return 0;
}
int msm_flash_lm3642_led_off(struct msm_led_flash_ctrl_t *fctrl)
{
int rc = 0;
struct msm_camera_sensor_board_info *flashdata = NULL;
struct msm_camera_power_ctrl_t *power_info = NULL;
LM3642_DBG("%s:%d called\n", __func__, __LINE__);
if (!fctrl || !fctrl->flashdata) {
pr_err("%s:%d fctrl NULL\n", __func__, __LINE__);
return -EINVAL;
}
flashdata = fctrl->flashdata;
power_info = &flashdata->power_info;
if (fctrl->flash_i2c_client && fctrl->reg_setting) {
rc = fctrl->flash_i2c_client->i2c_func_tbl->i2c_write_table(
fctrl->flash_i2c_client,
fctrl->reg_setting->off_setting);
if (rc < 0)
pr_err("%s:%d failed\n", __func__, __LINE__);
}
gpio_set_value_cansleep(
power_info->gpio_conf->gpio_num_info->
gpio_num[SENSOR_GPIO_FL_NOW],
GPIO_OUT_LOW);
return rc;
}
int msm_flash_lm3642_led_low(struct msm_led_flash_ctrl_t *fctrl)
{
int rc = 0;
struct msm_camera_sensor_board_info *flashdata = NULL;
struct msm_camera_power_ctrl_t *power_info = NULL;
LM3642_DBG("%s:%d called\n", __func__, __LINE__);
flashdata = fctrl->flashdata;
power_info = &flashdata->power_info;
gpio_set_value_cansleep(
power_info->gpio_conf->gpio_num_info->
gpio_num[SENSOR_GPIO_FL_NOW],
GPIO_OUT_HIGH);
if (fctrl->flash_i2c_client && fctrl->reg_setting) {
rc = fctrl->flash_i2c_client->i2c_func_tbl->i2c_write_table(
fctrl->flash_i2c_client,
fctrl->reg_setting->low_setting);
if (rc < 0)
pr_err("%s:%d failed\n", __func__, __LINE__);
}
return rc;
}
int msm_flash_lm3642_led_high(struct msm_led_flash_ctrl_t *fctrl)
{
int rc = 0;
struct msm_camera_sensor_board_info *flashdata = NULL;
struct msm_camera_power_ctrl_t *power_info = NULL;
LM3642_DBG("%s:%d called\n", __func__, __LINE__);
flashdata = fctrl->flashdata;
power_info = &flashdata->power_info;
gpio_set_value_cansleep(
power_info->gpio_conf->gpio_num_info->
gpio_num[SENSOR_GPIO_FL_NOW],
GPIO_OUT_HIGH);
if (fctrl->flash_i2c_client && fctrl->reg_setting) {
rc = fctrl->flash_i2c_client->i2c_func_tbl->i2c_write_table(
fctrl->flash_i2c_client,
fctrl->reg_setting->high_setting);
if (rc < 0)
pr_err("%s:%d failed\n", __func__, __LINE__);
}
return rc;
}
static int msm_flash_lm3642_i2c_probe(struct i2c_client *client,
const struct i2c_device_id *id)
{
struct msm_camera_sensor_board_info *flashdata = NULL;
struct msm_camera_power_ctrl_t *power_info = NULL;
int rc = 0 ;
LM3642_DBG("%s entry\n", __func__);
if (!id) {
pr_err("msm_flash_lm3642_i2c_probe: id is NULL");
id = lm3642_i2c_id;
}
rc = msm_flash_i2c_probe(client, id);
flashdata = fctrl.flashdata;
power_info = &flashdata->power_info;
rc = msm_camera_request_gpio_table(
power_info->gpio_conf->cam_gpio_req_tbl,
power_info->gpio_conf->cam_gpio_req_tbl_size, 1);
if (rc < 0) {
pr_err("%s: request gpio failed\n", __func__);
return rc;
}
if (fctrl.pinctrl_info.use_pinctrl == true) {
pr_err("%s:%d PC:: flash pins setting to active state",
__func__, __LINE__);
rc = pinctrl_select_state(fctrl.pinctrl_info.pinctrl,
fctrl.pinctrl_info.gpio_state_active);
if (rc)
pr_err("%s:%d cannot set pin to active state",
__func__, __LINE__);
}
if (!rc)
msm_lm3642_torch_create_classdev(&(client->dev),NULL);
return rc;
}
static int msm_flash_lm3642_i2c_remove(struct i2c_client *client)
{
struct msm_camera_sensor_board_info *flashdata = NULL;
struct msm_camera_power_ctrl_t *power_info = NULL;
int rc = 0 ;
LM3642_DBG("%s entry\n", __func__);
flashdata = fctrl.flashdata;
power_info = &flashdata->power_info;
rc = msm_camera_request_gpio_table(
power_info->gpio_conf->cam_gpio_req_tbl,
power_info->gpio_conf->cam_gpio_req_tbl_size, 0);
if (rc < 0) {
pr_err("%s: request gpio failed\n", __func__);
return rc;
}
if (fctrl.pinctrl_info.use_pinctrl == true) {
rc = pinctrl_select_state(fctrl.pinctrl_info.pinctrl,
fctrl.pinctrl_info.gpio_state_suspend);
if (rc)
pr_err("%s:%d cannot set pin to suspend state",
__func__, __LINE__);
}
return rc;
}
static struct i2c_driver lm3642_i2c_driver = {
.id_table = lm3642_i2c_id,
.probe = msm_flash_lm3642_i2c_probe,
.remove = msm_flash_lm3642_i2c_remove,
.driver = {
.name = FLASH_NAME,
.owner = THIS_MODULE,
.of_match_table = lm3642_i2c_trigger_dt_match,
},
};
static int __init msm_flash_lm3642_init(void)
{
LM3642_DBG("%s entry\n", __func__);
return i2c_add_driver(&lm3642_i2c_driver);
}
static void __exit msm_flash_lm3642_exit(void)
{
LM3642_DBG("%s entry\n", __func__);
i2c_del_driver(&lm3642_i2c_driver);
return;
}
static struct msm_camera_i2c_client lm3642_i2c_client = {
.addr_type = MSM_CAMERA_I2C_BYTE_ADDR,
};
static struct msm_camera_i2c_reg_setting lm3642_init_setting = {
.reg_setting = lm3642_init_array,
.size = ARRAY_SIZE(lm3642_init_array),
.addr_type = MSM_CAMERA_I2C_BYTE_ADDR,
.data_type = MSM_CAMERA_I2C_BYTE_DATA,
.delay = 0,
};
static struct msm_camera_i2c_reg_setting lm3642_off_setting = {
.reg_setting = lm3642_off_array,
.size = ARRAY_SIZE(lm3642_off_array),
.addr_type = MSM_CAMERA_I2C_BYTE_ADDR,
.data_type = MSM_CAMERA_I2C_BYTE_DATA,
.delay = 0,
};
static struct msm_camera_i2c_reg_setting lm3642_release_setting = {
.reg_setting = lm3642_release_array,
.size = ARRAY_SIZE(lm3642_release_array),
.addr_type = MSM_CAMERA_I2C_BYTE_ADDR,
.data_type = MSM_CAMERA_I2C_BYTE_DATA,
.delay = 0,
};
static struct msm_camera_i2c_reg_setting lm3642_low_setting = {
.reg_setting = lm3642_low_array,
.size = ARRAY_SIZE(lm3642_low_array),
.addr_type = MSM_CAMERA_I2C_BYTE_ADDR,
.data_type = MSM_CAMERA_I2C_BYTE_DATA,
.delay = 0,
};
static struct msm_camera_i2c_reg_setting lm3642_high_setting = {
.reg_setting = lm3642_high_array,
.size = ARRAY_SIZE(lm3642_high_array),
.addr_type = MSM_CAMERA_I2C_BYTE_ADDR,
.data_type = MSM_CAMERA_I2C_BYTE_DATA,
.delay = 0,
};
static struct msm_led_flash_reg_t lm3642_regs = {
.init_setting = &lm3642_init_setting,
.off_setting = &lm3642_off_setting,
.low_setting = &lm3642_low_setting,
.high_setting = &lm3642_high_setting,
.release_setting = &lm3642_release_setting,
};
static struct msm_flash_fn_t lm3642_func_tbl = {
.flash_get_subdev_id = msm_led_i2c_trigger_get_subdev_id,
.flash_led_config = msm_led_i2c_trigger_config,
.flash_led_init = msm_flash_lm3642_led_init,
.flash_led_release = msm_flash_lm3642_led_release,
.flash_led_off = msm_flash_lm3642_led_off,
.flash_led_low = msm_flash_lm3642_led_low,
.flash_led_high = msm_flash_lm3642_led_high,
};
static struct msm_led_flash_ctrl_t fctrl = {
.flash_i2c_client = &lm3642_i2c_client,
.reg_setting = &lm3642_regs,
.func_tbl = &lm3642_func_tbl,
};
module_init(msm_flash_lm3642_init);
module_exit(msm_flash_lm3642_exit);
MODULE_DESCRIPTION("lm3642 FLASH");
MODULE_LICENSE("GPL v2");