Hello,
i am thinking to use BQ24165 for one of our design where we have a DC source of 5V needing to charge Lithium battery. The system has to be able to switch between battery power the system or DC source power the system based on if there is DC source present or not.
I have spotted the BQ24165 but I am not fully sure the system can be powered by the battery as back up by switching automatically ornot. Does anyone can confirm this ?
I am also looking at reference design for this chip.