having an issue with this board not regulating current properly. to prevent damage we tested as follows limiting current from power supply.
test observations:
we've modified this board to drive LEDs other than on-board ones (cut trace between board LEDs and ground, added wires to go off-board). the DIMM signal is tied to V-in through a 100 kOhm resistor. V-in is set to 5.0 V and current limit on power supply is set to zero. monitoring LED current and V-FB (and they track each other as they should with 1 ohm resistor on board). R4 not installed.
upon increasing current limit on power supply, current will begin to flow and LED lights up and power supply voltage shows 2.0-2.1 V output. further increase on current limit causes LED current to increase toward limit (190 mA) with no change in output voltage (2 V). as we approach 190 mA LED current the current will suddenly increase to 350-400 mA (didn't let it run long) and nearly full V-in of 5 V.
Questions:
1-don't understand why current is not being regulated to 190 mA as this is purpose of the device. suggestions?
2-are there any other tests which would help explain this behavior?
3-what other ways can we make the board function as needed, other than putting PWM on DIMM pin (which would be a PITA).
thanks