Other Parts Discussed in Thread: BQ25120
Hello I have a problem with the right settings of the bq25120,
In the default settings of the bq25120 there are 1.8V on the SW pin. And now my question: If I set the output Voltage from the default 1.8V to 3.3V over I2C. Then a communicate over I2C is furthermore possible, when the I2C-Pullup-Resistors are furthermore powered from a Power-Supply of 1.8V. Or should I also change the Voltage of the I2C-Pullups-resistors if I change the default output-voltage from 1.8V to 3.3V.