Hello all,
we have to design an 5V,approx 200ma output with Bq51013B/Bq51003B. we need to have a ultra-compact very thin solution. we have designed with 0603 capacitors and resistors and the circuit works. now we would like to know, will the design works, when 0603 caps are replaced with 0402 or 0201 capacitors of same values 50V rated capacitors with DSBGA package. we are looking for almost 5mmx5mm or 4mmx8mm solution with 2 layer flex PCB.so we need to shrink the design. can the circuit works properly if we choose lower size components.
Thank u