I am in search for a boost converter that will do following:
Vin = 5V ~ 5.3V
Vout = 6V
Iout = 2A min , the load will pull 1.8A
built in switch
load disconnect when disabled
low quiescent current
Thank you!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Chris,
You can use TPS61089 plus an external MOSFET to realize this function. I wrote an reference design PMP9779, but this design has not been released yet. But I can send the schematic to you if you want it.
Also , you can use TPS61178, this device has load disconnect function , we already have the samples on hand now. But this device will be RTMed (officially released) early next year, can this meet you schedule?
you can wrote to me by email: helen-chen@ti.com
BR,Helen