Hi,
We want to implement a lead acid battery charger the BQ24702 chip, this since the IC is less expensive than other options and also because it has extra features we found important for our design such as adapter current measurement. Basically we will be charging a 12V lead acid battery between 7 to 10 Ah, the idea is to control the charge current setting by having different voltage dividers on the SRSET pin controlled by an MCU. On pre-charge we are thinking in use a charge current of 100mA, for normal charge 1A and for fast charge 2A. Also we are thinking in change the BATP pin voltage so we can change from the constant voltage phase (14.4V) to float phase (13.6V). We will add a current sense IC to measure the charge current and be able to detect the moment to change from constant voltage phase to float phase. Also we are going to be able to measure the battery voltage, so the MCU will have voltage a current readings in order to decide when change the charger current and voltage.
the questions we have are:
1) In your expert opinion, the implementation above is feasible?
2) Making the calculation for the inductor, we plan to make them for the normal charge current of 1A and a 20% of ripple. This give us a 33uH inductor, doing the calculation for 0.1A and 2A we notice that for 0.1A the current ripple will be too high, is this ok? I mean, the charger data sheet explain you can use a precharge by changing the voltage at the SRSET pin but it does not explain the implication this have over the current ripple.
Best regards