This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65400 - PGOOD status when current sharing or one switch OFF

Other Parts Discussed in Thread: TPS65400

Hello,

I want to use the TPS65400 *without programming* (only default values).

If I understand the DS, by default PGOOD output is the logical AND of individual PGOODs.

It's not clear if individual PGOOD is automatically masked when an output is disabled (ENSWx=0) : will PGOOD pin be asserted (tristated) when using for example only three channels ? If not, what is the solution to have PGOOD asserted when all *ACTIVE* outputs are OK, and without programming ?

Independantly, in case of Current Sharing, it seems that slave individual PGOOD is not masked so PGOOD pin will never be asserted when using this mode, right ? So, same question, how can I get PGOOD asserted when using current sharing, and without programming ?

Proposition : what if I connect VFB of an inactive or slave channel to the VFB of an active or master channel, will the individual PGOOD be OK so that the global PGOOD will be asserted ?

Thanks in advance