Hi everyone,
Sorry if the question has already been asked, but I can't find it.
I'm looking to drive a micro vibrating motor like this : http://www.smt-sanyo.co.jp/english/products/pdf/vibration.pdf
The 3089 precisely, 2.7V nominal voltage, 90mA peak current. It is possible to drive it directly with the TPS78227 LDO?
I juste have to add the two uF capacitors required, no diode or other protective circuit?
Best regards