I’m wondering if I can use a gate driver (Texas Instruments, UCC27536) to convert logic level data to 27 Volt logic level data? There’s some capacitance I need to drive (100nF) but I believe I should be able to get pretty good risetimes (better then 1usec). Also, if I need to charge a battery can the same driver handle continuous currents of ~ 1 Amp?