Hi TI team,
We are using Exide 12V 7Ah battery in our application.After making sure that battery is in rest mode for long enough we have given IT_Enable command.Immediately learned and update status changed to 04 and also VOK and QEN are set. So started charging battery to it's charge termination voltage 14.7V during which VOK and RUP_DIS are cleared.After attaing charge termination voltage and current being reached below taper current and above quit current stooped charging the battery where OCVTAKEN is set and FIRSTDOD are cleared.But VOK is not yet set again and also no updation in Learned,Update and Max Error values.Could you please suggest when to start discharging phase of the cycle and what are parameters to be taken care for successful completion of this learning cycle to get acknowledged that Qmax and Ra tables are set correctly