Hello All,
I would like to use a controller for DC input of 12V-30V and output of 16 VDC, 2A.
I prefer to use primary side regulated flyback for it's simplicity, but not averse to using any other isolated topology.
I checked on UCC2863x family,UCC287xx family. When I enter the input and output values on their design calculators, many values in the calculated outputs turn to negative values or RED. I guess they can work with only AC line range.
I also checked on UC3842a. It's description seems to match with my requirement,but 'WEBWNCH' returns 'Vin out of range' when I insert my input range.
Can anybody clarify if above controllers can be used with Vin range of 12V-30V DC ( OR corresponding Vac-rms ?
If they cannot be used, which are better suited to my requirement ?
Thanks in advance,
Param.