This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

force BQ27505 to determine SOC

Hi,

is there any way to force the BQ27505 to determine new SOC programmatically? In high temperature condition happens the fuel gauge reports 100% SOC when the voltage is only 3.7V.

My battery has 6200mAh capacity at 4.2V.

 

Thanks

  • Hi Luca,

    Does the gauge work as expected for you at room temp?

    First, can you confirm that you successfully configured the gauge to work with your battery by going through the bqEASY wizard in the evaluation software?

    If not, I would expect the behavior that you reported.  How much capacity is it reporting in mAh when you reach 100% SOC?

    To answer your specific question, yes, you can force it to take an open-circuit voltage reading and recalculate the current SOC with the Control(OCV) command, but this may not be the right way to solve your problem.

    If you like, you can post your GG file and a log of your charge cycle and I'll review it to see if there is some explanation in them.

  • Hi,

    I did a mistake in my previous message, the test wasn't conducted at high temperature condition. The ambient temperature was going from -10C to 60C and the device has been powered on at about 40C.

    The gauge works as expected at room temp and has been configured using bqEasy wizard.

    The data recorded are:

    Status: 0x0A80

    OpConfig: 0x8973

    SOC: 100%

    Remaining cap: 6647mAh

    Battery temp: 11°C

    Battery level: 3,476V

    Min battery discharge: 3200mV

    Max battery voltage: 4200mV

    Battery temp range: -10°C to 60°C

     

    Thanks

    Regards

     

    Luca

  • Can you explain the actual test in more detail, please?

    For example:

    Connect battery at 25degC, allow gauge to initialize

    Starting SOC =?%

    Begin charging at 3A at 25degC

    Ramp temperature to -10degC at 1degC/minute

    Ramp temperature to 60degC at 1degC/minute

    Soak at 60degC until charging is complete

     

    Are you sure your battery allows charging at these extreme temperatures?  Please check the battery spec.