This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello all,
I have a unit with following input power supplies: (1) +7V with 0.4A, (2) +5V with 0.2A and (3) -5V with 0.06A.
I have to switch-off the unit with a DO from a controller. This controller is operating on a separate power supply.
Any of the CSD13302W, CSD13306W, CSD13383F4 or CSD83325L will suite for my application? Further any driver device is required?
Can anybody suggest me the suitable circuit please?
Thanks in advance.
Dear Brett,
In my application, FETs are proposed to act as load switch.
Can you please suggest me the best suitable FET for my application?
Is there any device required to drive the FET in High-side configuration?