Hi,
We are designing a 12V input to 48V for 3A output application.
Is there any thermal performance for this condition that can share with us?
Thanks a lot.
Best regards, Cage.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
At 12 V input, the p-p inductor ripple current is 10.14 A. That is relatively a lot compared to the 2.5 A output current. Typically flat wire inductors do not perform well thermally with large ac ripple currents, even though the dc losses are small. That is most likely why the inductor is heating up so much. I will forward this to the circuit designer for his comment.
Hi Cage,
Thank you for contacting us.
You are correct, the image on pg5 looks suspicious, at min Vin of 12Vin, the peak current is the highest and this will reflect on the low side switch FET. I built another same board, and re-run the thermal, the result makes sense, please see attached. This new image will be updated on TI.com within the next couple days.
Please let us know if there is anything we can help to design the LM5122 for you.
Best regards,