Hello,
First of all, I want to clarify that I'm a beginner at designing flyback SMPS, and our company (from Argentina), is recently dabbling into this field. So, we're currently working in a USB charger design with an output power of 10W. Among the different providers, we came across 2 IC from TI which are UCC28911 and UCC28704. Our aim is to manufacture the charger using an IC with an integrated MOSFET to accomplish a compact design (that is to say, UCC28911). However, from the datasheet of this device (SLUS769C), I cannot understand if it's viable for the application at issue (below is attached the chart with the specifications). The AC input voltage for the charger will be in the range of 90VAC to 265VAC.
In short, I would like to know if we can use UCC28911 in a 10W USB charger, or, do we have to use the UCC28704 with an external MOSFET?
Thanks in advance,
Best regards.