This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PTN78060W

Hi,

   I recently purchased the PTN78060WAZT, and I am wondering if the development board has built in Cin, Cout and Rset?

If not, Can I use a 2.2uF ceramic cap with 100V rating, and 100uF ceramic for the Cout?

Thanks,

Hoa

  • Hoa:

    PTN78060WAZT requires a 2.2uF ceramic capacitor on  the  input pins. The input ceramic recommended  minimum voltage rating is 50Vf it is X5R tolerance. Any other  tolerance voltage rating is > 60V.

    The required minimum  output capacitance is 100uF polarized  type, plus  optional output ceramic capacitances is limited to 200uF.

    Tom