Part Number:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Ali,
Sorry for the parameters that were left off. The resistors (R1, R5, R6, R7) should be 1%.
The MMBT3904 transistor is 60V, 200mA, 350mW
The MMBT3906 transistor is -40V, 200mA, 350mW
Thanks,
Robert